Forterra

Developing life-saving autonomy technology for the Department of Defense

Company

Forterra (formerly RRAI)

Company Maxim

Groundbreaking, Ground-based Autonomy

Challenge

Creating ground autonomy for unstructured, complex environments

Location

Clarksburg, Maryland, United States

Products used

"Delivering water and supplies should not be a life threatening mission."

The long supply chains that are a necessity in any military operation are some of the most vulnerable, and some of the first that can be protected with autonomy technology. Simple tasks like delivering water and fuel to sustain forces can be a life-threatening mission. Forterra (formerly RRAI) develops ground-based vehicle autonomy for the defense sector to get drivers out of those seats.

The Challenge

Off-road driving in combat environments comes with its own set of obstacles: no lane markings and unfamiliar terrain. DoD ground vehicles need to traverse complex design domains, such as extreme temperature and GPS-degraded denied regions, and low-light and weather-impaired environments. These requirements necessitate an autonomy platform that is flexible, rugged, and reliable across roadway conditions.

The Solution

Core to the way that Forterra’s autonomy platform, AutoDrive, operates is its perception stack, which is largely built around lidar. Forterra’s AutoDrive platform is equipped with multiple OS digital lidar sensors from Ouster for maximum visibility around the vehicle, in addition to cameras and radar. Defense applications are often working in foggy, dusty and rainy environments, and lidar is the key enabling sensor for the autonomy system to navigate effectively and safely in the harshest conditions.

Forterra’s autonomous capabilities are being applied to military vehicles on and off-road, as well as commercial trucks. Forterra was selected to develop systems for four active DoD programs:

  • Robotic Combat Vehicle (RCV) program

  • Autonomous Transport Vehicle System (ATV-S) program (also known as the the Ground Expeditionary Autonomous Retrofit System or GEARS)

  • Remotely Operated Ground Unit for Expeditionary Fires (ROGUE Fires) program

  • Squad–Multipurpose Equipment Transport (SMET) program

Forterra’s autonomy platform will help America’s Armed Forces safely conduct reconnaissance, troop supply missions, and related tasks during ground warfare to keep soldiers out of harm's way. Forterra has shipped over 100 vehicles, operating a cumulative 400,000 miles. Its technology is currently operating in U.S. military programs in over ten countries.

Ouster is committed to the responsible use of lidar technology. For more information on our policy regarding the use of our products for military and security applications, see Ouster’s Engagement and Responsible Use Principles.

Product Used

Powered by the L3 chip to deliver best-in-class point cloud density and range, the OS series offers clean, dense data across its entire field of view for accurate perception and crisp mapping.

Product Used

Powered by the L3 chip to deliver best-in-class point cloud density and range, the OS series offers clean, dense data across its entire field of view for accurate perception and crisp mapping.
  • Get Sample Data

    View sample data from rugged, off road, weather impaired environments like the ones where Forterra is operating

Case Studies to explore

Ouster sensors are used by 600 customers worldwide, from raw material to last mile delievery, and everything in between.