Get the telemetry information
Get the sensor telemetry information
Response
Valid telemetry query result
timestamp_ns
Time at which the information was collected
phase_lock_status
The current phase-lock status will not indicate loss of lock if the time synchronization is lost.
input_voltage_mv
Reports system input-voltage in millvolts
internal_temperature_deg_c
Reports system temperature in degrees C
Only available on Rev 06 and above sensors.
input_current_ma
System input-current in milliamps