Get the IMU data format

Open in Claude

Get the sensor IMU data format.

Note: User can run DELETE /api/v1/sensor/config command to configure imu_data_format back to default i.e. NORMAL. For more information on the IMU specifications refer to Sensor Datasheet.

Response

IMU packet structure metadata
accel_fsrenum
Refers to the Full Scale Range of the accelerometer
gyro_fsrenum
Refers to the Full Scale Range of the gyroscope
imu_packets_per_frameenum
IMU packets per frame
imu_rate_hzenum
Configured IMU sample rate in hertz
imu_measurements_per_packetinteger
IMU measurements per packet
udp_profile_imuenum
The configured UDP profile for IMU