Get the system network configuration
Get the system network configuration
Response
System network configuration
carrier
State of Ethernet link, true when physical layer is connected
duplex
Duplex mode of Ethernet link, half or full
ethaddr
Ethernet hardware (MAC) address.
hostname
Hostname of the sensor, also used when requesting DHCP address and registering mDNS hostname
ipv4
ipv6
speed
Ethernet physical layer speed in Mbps, should be 1000 Mbps