Cold Start
Cold-start allows the sensor to self-heat before entering normal operation when it detects a low environmental temperature.
Note: For Rev 7 Sensors, please use FW 3.0.0 and later.
Hardware Requirements
Gen 1 sensors are not cold-start-compatible on any firmware. All sensors enter the warmup state at low temperatures, but only Gen 2 sensors successfully exit warmup into normal operating state.
Cold Start Operation
No configuration change is required. The sensor automatically warms up at the cold end of its operating temperature range.
Indications and Alerts
During cold start, the sensor emits a "WARMUP" status to indicate it is in the warmup phase.
The following alerts are related to cold start: