Linux
Tested on Ubuntu 18.04 and 20.04.4 LTS. The sensor hostname is os-991234567890.local (serial number on the sticker on top of the sensor).
Connecting the Sensor
- Connect the sensor to an available Ethernet port on the host machine or router.
- The sensor automatically obtains an IP address via link-local or DHCP, depending on network configuration.
- When connecting directly to the host machine, set the Ethernet interface to
Link-Local Onlymode via CLI or GUI. See Setting the Interface to Link-Local Only.
Note: It can take up to 60 seconds to obtain an IP address after initial power-up.
Setting the Interface to Link-Local Only
Via Command Line:
Command
Note: To find your connection name, run
nmcli connection show.
Example — with interface name eth0:
Response: (no output)
Note: Verify the change with
ip addr. Once the sensor is reconnected, theinetline foreth0will show the negotiated link-local address (e.g.,169.254.1.100).
Via GUI: Set the interface to Link-Local Only mode in the network manager GUI.
The Sensor Homepage
- Enter
http://os-991234567890.local/in your browser’s address bar to open the sensor homepage.
Note: If the sensor homepage does not load, follow the steps in Determining the IPv4 Address of the Sensor to verify the sensor has a valid IP address.
Determining the IPv4 Address of the Sensor
-
Open a Terminal (Ctrl+Alt+T).
-
Ping the sensor to find its IPv4 address:
Command
Example
Note: If this command hangs, configure your interface to link-local first (see Setting the Interface to Link-Local Only).
Response
Note: In this example, the sensor IPv4 address is
192.0.2.130. An address of the form169.254.x.xmeans it is connected via link-local.
- Alternatively, browse by service type using
avahi-browse:
Command
Example
Response
Note: An address of the form
169.254.x.xmeans the sensor is connected via link-local.
Determining the IPv4 Address of the Interface
Identify the IPv4 address of the interface the sensor is connected to (e.g., eth0 in the example below).
-
Open a Terminal (Ctrl+Alt+T).
-
View all interface addresses:
Command
Example
Response
- In this example, the sensor is plugged into interface
eth0. - The host IPv4 address is on the
inetline — here,169.254.1.100.
Note: An interface address of the form
169.254.x.xmeans Linux self-assigned a link-local address in the absence of a DHCP server.
Setting the Host Interface to DHCP
Set the interface to obtain an IP address automatically via DHCP.
Note: Unplug the cable from the interface before making changes.
Via Command Line:
Command
Example — with interface name eth0:
Response: (no output)
Note: Verify the change with
ip addr. Theinetline foreth0will be absent until a cable is connected to a device with a DHCP server.
Via GUI: Set the interface to Automatic (DHCP) mode in the network manager GUI.
Setting the Host Interface to Static IP
Assign a static IPv4 address to the interface.
Note: Unplug the cable from the interface before making changes.
Via Command Line:
Command
Example — with interface eth0 and IPv4 address 192.0.2.1/24:
Note:
/24is shorthand for Subnet Mask255.255.255.0.
Response: (no output)
Note: Verify the change with
ip addr. Theinetline foreth0will show the static address, e.g.,192.0.2.1.
Via GUI: Set the interface to Manual (static) mode in the network manager GUI.
Finding a Sensor with mDNS Service Discovery
The sensor announces itself via mDNS with service type _ouster-lidar._tcp. Use avahi-browse to find all sensors on the network.
- Find all sensors and their IPv4 addresses using service type
_ouster-lidar._tcp:
Command
Example
Response
Note: In this example, the sensor IPv4 address is
192.0.2.130.